Cancel Promoted Scanning

Associated with: Direct or Shared outstations

Security permission required to access this pick action: Promote

This pick action is only available if the rate at which an outstation is being scanned is currently promoted (see Promote Scanning).

Use the pick action to terminate the current promotion. Once executed, ClearSCADA reverts to scanning the outstation at its usual scan rate.


Disclaimer

ClearSCADA 2017 R2