Current Value

Associated with: Points

This status attribute displays a point’s current value (rather than its Current State).

Use the attribute in conjunction with other attributes, such as Current Quality to assess the reliability of the point’s data.

(The possible values for a point are specified on a per-point basis, on the corresponding Point Form.)

Also see Previous Update Value.


Disclaimer

ClearSCADA 2017 R2