Dial In Overactive Alarm

Associated with: PSTN outstations or outstations on which PSTN fallback is enabled

This status attribute is only displayed for outstations on which the Dial In Overactive feature is enabled (see Define Dial In Overactive Properties on a PSTN Outstation in the ClearSCADA Guide to Advanced Drivers).

The status attribute indicates whether the outstation is currently overactive and dialing in too often. The attribute automatically reverts to Enabled Inactive at the end of each dial-in period. (The period is specified on the PSTN tab of the Outstation Form).

Possible states: Displays one of the Standard Alarm States.

An alarm condition indicates that the outstation is deemed to be dialing in to the server too often. Refer to the Dial In Overactive attribute for the maximum number of calls that the outstation is expected to instigate, compared to the actual number of calls that have occurred so far.


Disclaimer

ClearSCADA 2017 R2