Dial Out Promoted
Associated with: Outstation sets; PSTN outstations or outstations on which PSTN fallback is enabled
This status attribute is only displayed if the Promote Dial Out feature is enabled for an outstation or outstation set (see Define an Outstation’s PSTN Properties in the ClearSCADA Guide to Advanced Drivers, or for sets, see Defining Communication Settings in the ClearSCADA Guide to Advanced Drivers).
The attribute indicates whether retrieval of data is currently promoted (occurring at a more frequent rate than usual) on the outstation or set.
Possible states:
- Yes
- No.
Further Information