Download Configuration
Associated with: Outstations on drivers that support configuration downloads.
Security permission required to access this pick action: Configure.
The Download Configuration option varies on some drivers - the driver-specific documentation explains any differences that apply to a particular driver.
UNEXPECTED BEHAVIOR OF APPLICATION
Use this pick action to download the configuration that is associated with an outstation, from the ClearSCADA database to that outstation (see Downloading Configuration Changes in the ClearSCADA Guide to Core Configuration).
The Download Config Alarm status attribute indicates the success, or otherwise, of the last Download Configuration request to the outstation.
The Download Configuration Required system color indicates when configuration changes have been made in ClearSCADA, which have not yet been downloaded to the relevant outstation.
If using this pick action with the Automation Interface, you need to specify the method name DownloadConfig.