Enable Channel

Associated with: Channels

Security permission required to access this pick action: Disable Points

Use this pick action to place a channel In Service. Triggering the action changes the channel's configuration so that its In Service property is enabled. Once enabled, the channel becomes active. If the channel is attached to a Direct Set, the outstations in that set will also become active (providing that the Direct Set and outstations are In Service and have valid configuration).

The Enable Channel pick action is only available for a channel:

Also see Disable Channel.

If using this pick action with the Automation Interface, you need to specify the method name Enable.


Disclaimer

ClearSCADA 2017 R2