Enable Outstation

Associated with: Outstations

Security permission required to access this pick action: Disable Points

Use this pick action to place an outstation In Service. Triggering the action changes the outstation's configuration so that its In Service property is enabled. Providing that the items on which the outstation is dependant are also In Service and have valid configuration, the outstation will become active. (Items on which the outstation is dependant include its outstation set and, for outstations other than PSTN outstations, a channel.)

The Enable Outstation pick action is only available for an outstation:

Also see Disable Outstation.

If using this pick action with the Automation Interface, you need to specify the method name Enable.


Disclaimer

ClearSCADA 2017 R2