Network
Associated with: Network-connected outstations and Slave outstations
The Network status attribute displays the outstation’s host address and port number, separated by a colon.
If a Dual Network is used, two entries are displayed—one for Network A and another for Network B.
The settings are as per those specified on the Network tab of the outstation’s configuration Form (see Define an Outstation’s Network Properties in the ClearSCADA Guide to Advanced Drivers).