No Change Alarm

Associated with: Points on which the No Change feature is enabled

Many types of point support ClearSCADA’s No Change feature (see Detect Whether a Point Value has Stopped Changing in the ClearSCADA Guide to Core Point Configuration). When this feature is enabled, the No Change Alarm status attribute indicates whether the point’s value has stopped changing.

Possible states: Displays one of the Standard Alarm States.


Disclaimer

ClearSCADA 2017 R2