Point Statistics
Associated with: Scanners; outstations; Slave outstations
This status attribute displays statistics about an outstation’s or scanner’s point data. The attribute lists the number of point updates, historic records, point alarms and events that ClearSCADA has retrieved from the outstation or scanner since the statistics were last reset.
24 updates, 26 historic, 0 alarms, 3 events since 11/Nov/2007 11:57:49.111
Also see Comms Statistics.
Further Information