Tune M/S Alarm Limits

Associated with: Analog points that are configured to use Master Station Alarm Limits

Use the Tune M/S Alarm Limits pick action to tune an analog point’s ‘master station’ alarm limits, as opposed to the point’s ‘standard’ alarm limits. The pick action is only available on an analog point on which:

You tune an analog point’s ‘master station’ alarm limits in a similar way to its ‘standard’ alarm limits (see Tune Alarm Limits). Unlike ‘standard’ tuning, ClearSCADA does not download any tuned ‘master station’ alarm limits to the outstation, as ‘master station’ alarm limits are used purely by the ClearSCADA server.

When you select the Tune M/S Alarm Limits pick action, the Tune M/S Alarm Limits window is displayed. The number and description of the fields that are displayed in the window varies, depending on the point’s configuration (the number of ‘master station’ alarm limits is configurable on a per-point basis).

The window indicates the limits that are currently in force. The point’s full range (Zero Scale to Full Scale) is displayed in parentheses on the right-hand side of the window.

Select the check boxes of those limit(s) that you want to tune and then specify the required temporary limits in the adjacent fields. Specify values that are within the range that is configured for the point.

Tuning does not change the values of the alarm limits on the point’s configuration Form.

When tuning is in force:

The 'Copy', 'Convert To', and 'Create Instance' features affect master station alarm limit tuning in the same way as 'standard' tuning (see Tune Alarm Limits).

To remove any tuning, display the Tune M/S Alarm Limits window and clear all of the check boxes. An entry will be logged in the Event Journal, stating that the Master Station Alarm Limits have been returned to their configured defaults.

NOTE: If using this pick action with the Automation Interface, you need to specify the method name TuneLimits. Ensure that you specify that the method is associated with the CPointAGLimits class (the Master Station Alarm Limits aggregate).


Disclaimer

ClearSCADA 2017 R2