ATAN (Inverse Tangent)
The ATAN function is a mathematical function that returns the inverse Tangent (radians) of a number. The ATAN function returns a real value.
Function Name |
ATAN |
Description |
Returns the inverse Tangent (radians) of a number. |
Arguments |
ATAN(INTEGER or REAL) The ATAN function can have one input and this can be either an integer or a real floating value—see Number (Integer or Real). |
Returns |
REAL The inverse Tangent (radians) value of the input. |
Example:
ATAN(1)
The output is 0.785
See also: