Configuration Fields
Some FloBoss Scanner object fields do not appear on the configuration form but are listed in the ClearSCADA Database Schema. These configuration fields are described below:
- Logging Level (Tag: $Config.LoggingLevel). This field controls the level of detail in the driver module’s log file for actions related to this scanner. A value of 0 means that the log file contains errors only and a value of 4 means that the log file is extremely verbose. For more information on logging, (see Driver Log File).