Example ClearSCADA Project File (FloBossDemo.SDE)

The example that is explained in these topics is available as a ClearSCADA database export (sde) file.

Once you have installed the ClearSCADA FloBoss Driver, you can optionally use the FloBossDemo.sde file to import the sample configuration into your database. You can then study the sample configuration to see how the FloBoss driver can be used to interface a FloBoss with ClearSCADA. The default location for the FloBossDemo.sde file is Program Files\Schneider Electric\ClearSCADA.

 

The demonstration file shows how to use the ClearSCADA FloBoss driver to:

 

After you successfully import the FloBossDemo.sde file, you should see a database tree similar to the one shown below. The topics that follow this one discuss various aspects of this sample database. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.


Disclaimer

ClearSCADA 2017 R2