How can I read a discrete input (DI) point from a FloBoss?

You need to configure a FloBoss Numeric Point with the correct Type, Location, and Parameter.

A DI point in a FloBoss has a Type of 1 and the Parameter that holds the actual DI value is 21 (EU value). The Location will depend on your specific hardware.

To read an accumulated value, read Parameter 5 (Accumulated Values) with Type = 1. The Location setting is hardware dependent.

For further information, (see FloBoss Numeric Point).


Disclaimer

ClearSCADA 2017 R2