MinuteHistory Mimic

The Mimics group in the FloBossDemo.sde contains a MinuteHistory Mimic.

This Mimic displays the minute history values, along with timestamps and a quality description for four runs from the FloBoss 107.  Click on a value on the Mimic to display the underlying point’s object menu. Use the menu options to view a historic List or a historic Trend to verify that the data was retrieved from the flow computer correctly.

You can exercise the driver by clicking a value, opening that point’s property menu, disabling history, verifying that the history is deleted, and then re-enabling history on the point. The driver will backfill the point data from the flow computer.

 


Disclaimer

ClearSCADA 2017 R2