Putting it all Together – A FloBoss Configuration Example

The topics in this section use an example database configuration to demonstrate how you can use the FloBoss Driver to interface ClearSCADA to a FloBoss 107 flow computer. The FloBoss 107 was chosen as it supports four meter runs and so is the more complex member of the FloBoss 100 family. FloBoss 103 and FloBoss 104 devices are a subset of the FloBoss 107.

The topics provide information about the example configuration that is contained in a ClearSCADA database export (sde) file, along with information about the various groups and database objects in that example configuration. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.


Disclaimer

ClearSCADA 2017 R2