Configure the Basic Scanner Properties

Use the fields on the Scanner tab of the appropriate Hilscher Scanner Form to define the general and Hilscher-specific properties for a Scanner. Many of the fields on this tab are common to scanners on many simple drivers—for information, see Configuring Scanners on Simple Drivers in the ClearSCADA Guide to Simple Drivers.

Fields that are common to Scanners on the Hilscher driver are described below. For fields that are not shown here, see the appropriate scanner-specific section within this guide.


Disclaimer

ClearSCADA 2017 R2