Configuring a Hilscher Board

On a DeviceNet or PROFIBUS-DP system, you need to configure a Hilscher Board in the ClearSCADA database for each physical Hilscher board that you want ClearSCADA to scan on your system.

On a PROFIBUS-FMS system, you need to configure a Hilscher Board in the ClearSCADA database for each I/O board through which ClearSCADA is to scan FMS devices.

In either case, specify the properties for a board using the Hilscher Board Form.

The Form has several tabs.

Use the Board tab to Configure the Basic Board Properties.

For fields on the other tabs, see Tabs That are Common to Many Configuration Forms in the ClearSCADA Guide to Simple Drivers. (These tabs have no driver-specific configuration settings.)


Disclaimer

ClearSCADA 2017 R2