Poll Times

Associated with: ICMP Digital Points

The Poll Times attribute indicates the number of times that the ClearSCADA server has polled the remote device since the Poll Statistics were last reset. It also indicates:

If the Poll Statistics have been reset, two sets of Poll Times attributes are displayed. The first displays the statistics since the last reset; the second displays the statistics between the previous two resets.

Example:

79 Polls, 79 Good, 0 Bad, Last 0.789206ms, Maximum 17.4098ms, Minimum 0.551467ms, Average 0.911682ms.


Disclaimer

ClearSCADA 2017 R2