ASDU

An Application Service Data Unit (ASDU) is a block of data that is sent from the Controlling Station (ClearSCADA) to an outstation or other device, or vice versa, using the IEC 60870-5 protocol.


Disclaimer

ClearSCADA 2017 R2