Configure Point Scaling

Use the fields within the Scaling section of the Analog Point tab to specify whether and how ClearSCADA scales the point values that are reported by the outstation.

Example:

If an outstation is reporting an analog point’s raw value as a Normalized Value (ID 9), you might specify a Raw Full Scale of +1 and Raw Zero Scale of -1.

If an outstation is reporting an analog point’s raw value as a Scaled Value (ID 11), you might use the Raw Full Scale and Raw Zero Scale fields to specify the required scaling, within the range +32767 and -32768.


Disclaimer

ClearSCADA 2017 R2