Delete File

Associated with: IEC 60870-5 Outstations

Security permission required to access this pick action: Configure

Use this pick action to delete a binary file on an IEC 60870-5 outstation.

Select the Delete File pick action to display the Delete File window. Use the fields in the window to specify the file that ClearSCADA is to delete.

Also see Get Directory.

If using this pick action with the Automation Interface, you need to specify the method name DeleteOSFile.


Disclaimer

ClearSCADA 2017 R2