Station Counter Interrogation Alarm

Associated with: IEC 60870-5 outstations

This attribute indicates whether the latest Request, Freeze and/or Reset request for the outstation’s counters has been unsucessful (see Understand and Resolve Outstation Interrogation Alarms).

The frequency with which ClearSCADA attempts to execute the above requests is specified as part of the outstation’s configuration (see Configure the Counter Interrogation Intervals).

Possible states: Displays one of the Standard Alarm States.


Disclaimer

ClearSCADA 2017 R2