Upload File

Associated with: IEC 60870-5 Outstations

Security permission required to access this pick action: Retrieve Data

Use this pick action to upload a binary file from an IEC 60870-5 outstation to the ClearSCADA server.

Select the Upload File pick action to display the Upload File window. Use the fields in the window to specify the file that ClearSCADA is to upload.

Further Information

see Get Directory


Disclaimer

ClearSCADA 2017 R2