Minimum Configuration

For an IEC 60870-5 KEMA Outstation to be capable of functioning, as a minimum you need to specify:

Also ensure that the outstation and the database items on which it depends are In Service, and have saved, valid configuration. This will produce an IEC 60870-5 KEMA Outstation that is capable of functioning using the default configuration settings.


Disclaimer

ClearSCADA 2017 R2