Terminology

Throughout this guide, the term ‘outstation’ is used to refer to any outstation, controller, or other device using the KEMA defined IEC60870-5-101 extension, used to obtain data from measuring instruments or sensors.

Throughout the ClearSCADA documentation suite ‘information objects’—the objects that can be monitored or controlled on an outstation—are referred to as ‘points’.

For information on this and other IEC 60870-5 terms with which you might need to be familiar in order to configure KEMA and IEC 60870-5 specific settings in ClearSCADA, see Terminology in the ClearSCADA Guide to the IEC 60870-5 Driver.


Disclaimer

ClearSCADA 2017 R2