IOA

Each input or output on an IEC 60870-5 outstation or other controlled device has an Information Object Address (IOA). This address is used to uniquely identify each item on the device and is transmitted in each ASDU that includes information about that particular input or output.


Disclaimer

ClearSCADA 2017 R2