Scanning Periods and Scan Phases

This section includes detailed information about scanning direct outstations on the Kingfisher driver. The section explains these processes and features, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.

If required, you can configure individual polling intervals and offsets on any direct outstations that the Kingfisher driver is not required to poll (scan) continuously—see Specify the Polling Intervals and Offset.

For further information on scanning direct outstations, see Scanning Process.


Disclaimer

ClearSCADA 2017 R2