Client-Specific Events List Preferences
This section summarizes those Events List options that a system administrator can configure on a per client basis. Such options, if required to differ from the defaults, should be specified on existing clients (workstations) when a ClearSCADA system is first installed, and then on new clients whenever they are added to the system. On each client, you specify the options using the Options window.
You can use the Options window to specify the format in which Lists are to be displayed on that particular client (see Specify the Preferred List Options on a ViewX Client).
For anyone that accesses the system without logging on via a User Account, use the Options window to define the client-specific Features that are available to the Guest User, including:
- Operational features, such as whether the Guest User actually has access to Events Lists on that particular client (see Define the Client Specific Settings for the Guest User in the ClearSCADA Guide to Security).