Fields that Perform Special Functions
Some database fields perform particular functions in ClearSCADA. Whenever these functions are required, the particular fields associated with those functions have to be included in the SELECT clause’s comma-separated list of fields. Unlike other database fields, these ‘special’ fields are not displayed as columns in the resultant List.
For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.