Set up Queries List Preferences
This section is for system administrators and high-level engineers who are setting up the preferences for Queries Lists on either a system-wide, client-specific, or user-specific basis (see Set up the List Preferences).
ClearSCADA is supplied with a set of predefined defaults for Queries Lists. These affect, for example, the List header colors. If required, these options can be changed from the defaults. Some of these options affect Queries Lists on a system-wide basis, whereas other options can be specified on a per-client (workstation) basis, or on a per-user basis.
For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.