Specify the Colors used in List and Alarm Banner Headers

Use the Header Colors section on the Option window’s Lists tab to specify the colors used in the header cells of Lists and the Alarm Banner:

To change any of the above:

  1. Click on the color that you want to change.
    A pop-up color window is displayed.
  2. Either:
    • Select a color from the palette.

      Or:

    1. Select the ... option.
      The Color window is displayed.
    2. Use the Color window to define a color (see Using the Color Window in the ClearSCADA Guide to Core Configuration).
    3. Select OK to close the Color window.
    4. Repeat the above steps for any other color that you want to change.
    5. Select the OK button at the bottom of the window to confirm the changes and close the Options window.

Example:

A ViewX client with this Header Color configuration:

Will result in List header cells that have these colors:


Disclaimer

ClearSCADA 2017 R2