Specify the Properties of the Font used in List Rows

This section only applies to Lists—for information on changing the font properties of the Alarm Banner, see Specify the Properties of the Font used for the Alarm Banner in the ClearSCADA Guide to Alarms.

Use the Row Font section on the Option window’s Lists tab to specify the properties of the font used in List rows:

Once you have confirmed the settings, you will need to close and re-open any Lists that are presently on display, in order for the changes to take effect on those Lists.


Disclaimer

ClearSCADA 2017 R2