System-Wide Historic List Preferences

This section summarizes those options that affect Historic Lists on a system-wide basis. Such options, if required to differ from the defaults, should be specified on each server when a ClearSCADA system is first installed. The options are specified using the ClearSCADA Server Configuration Tool.

You can use the ClearSCADA Server Configuration Tool to specify:


Disclaimer

ClearSCADA 2017 R2