Time Formats for Filters

If you filter a List by a database field that represents a time, you are offered a predefined choice of base times, or time intervals (see Filter Condition Types) in the Add Filter window or Edit Filter window. If you want to specify a different base time, or time interval to those on offer, select the Relative Time, Relative Times, Specific Time, or Specific Times option.

Whether you select a predefined option, or opt to enter your own time criteria, ClearSCADA is capable of interpreting two time formats when filtering a List:

Further Information

Specifying a user’s Date Format: see Define the Regional Settings for a User in the ClearSCADA Guide to Security.

Configuring the Guest and Web User Accounts in the ClearSCADA Guide to Security.


Disclaimer

ClearSCADA 2017 R2