Binary Values

Digital values (binary values) are stored in bit strings. There are 5 types of bit string.

When you need to use a binary value in your Logic program, you have to define the type of binary value and the actual value. For more information, see Binary Value Types and see Binary Value Formats.


Disclaimer

ClearSCADA 2017 R2