Built-In Data Types

There are many different types of built-in value (literal value) that you can add to your Logic programs.

For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.

The built-in value types, sometimes referred to as literal data types, use a specific name to define the data type. For example, text values are STRING values. You can use Derived Data Types to allocate different names to value types.


Disclaimer

ClearSCADA 2017 R2