Create a Function Block Diagram Database Item
Each Function Block Diagram needs to be represented in the ClearSCADA database by a Function Block Diagram item. When you have created a Function Block Diagram item, you can access its Edit feature which allows you to create the Function Block Diagram program.
To create a Function Block Diagram database item:
- Display the Database Bar (see Display an Explorer Bar).
- In the Database Bar, right-click on a system, Group, or Group Template to display a context sensitive menu.
- Select the Create New option, then the Logic option, then the Function Block Diagram option from the context sensitive menu.
A new Function Block Diagram item is added to the system, Group, or Group Template. It is selected automatically, ready for you to enter its name. - Enter a suitable name for the Function Block Diagram then press the Enter key or select another part of the interface.
Now that you have created a Function Block Diagram database item, you can edit it (see Edit a Function Block Diagram).