DT_TO_DATE

Function Name

DT_TO_DATE

Description

Converts a Date and Time input into a Date output (the output will not include a time).

Arguments

Input 1 {DATE_AND_TIME}

For more information on the data types for the inputs and outputs, see Data Type Hierarchy.

Returns

Output {DATE}

The output is the result of Input 1 - the Time supplied by Input 1.

Example:

Function Block Diagram - DT_TO_DATE:

A DT_TO_DATE function has an input of NOW. This sets the input to be the current date and time. The DT_TO_DATE function returns the date part of the input as its output.

ST Program - DT_TO_DATE:

The syntax for a DT_TO_DATE function in an ST Program is:

Output := DT_TO_DATE (Input 1)

Where Output is a Date value and Input 1 is a Date and Time value.


Disclaimer

ClearSCADA 2017 R2