Define whether a Logic Program Executes when the Value of an Input Changes

If a Logic program is configured to have an Execution Method setting of On Interval, you can configure the system to automatically execute the program whenever one of the program’s inputs changes value. This is useful, as it means you can set a Logic program to execute on a timed basis, but only if its inputs have changed value.

To choose whether a Logic program executes only when its inputs have changed, you need to use the Input Change Detection check box on the Logic tab of Logic Program Form:

Further Information

Display the Logic Program Form: see Configure an ST Program, Ladder Diagram, SFC or FBD.


Disclaimer

ClearSCADA 2017 R2