Edit a Function Block Diagram

You can display a Function Block Diagram in Design mode by double-clicking on a Function Block Diagram item in the Database Bar. In Design mode, you can edit the Function Block Diagram by adding or removing values and components such as functions.

To edit a Function Block Diagram, either:

Or:

The Function Block Diagram is displayed in the ViewX Application window (see Function Block Diagram Display).


Disclaimer

ClearSCADA 2017 R2