Logic Program Properties and Values

Each type of Logic program is represented in the database by a database item. Like other database items, ST Programs, ST Libraries, Function Block Diagrams, Ladder Diagrams, and Sequential Function Charts have configuration Forms.

To learn about the settings that are available on ST Program, Ladder Diagram, Function Block Diagram, and Sequential Function Chart Forms, see Configure an ST Program, Ladder Diagram, SFC or FBD.

To learn about the settings that are available on the ST Library Form, see Configure an ST Library.

As with other types of database item, the Logic programs also have OPC tags for their configuration properties. You can view these tags by using the OPC Data Bar (see OPC Properties for Logic Programs).


Disclaimer

ClearSCADA 2017 R2