MUL

Function Name

MUL (Multiply)

ST Operator

*

Description

Multiplies the inputs to provide the output.

Arguments

Input 1 - Input n {ANY_NUM}

For more information on the data types for the inputs and outputs, see Data Type Hierarchy.

Returns

Output {Same data type as input}

The Output = Input 1 x Input 2 x Input 3 and so on.

Example:

Function Block Diagram - MUL:

The output is the result of the top input multiplied by the bottom input. So, if the top input is 2 and the bottom input is 19, the output is 38 (2 x 19=38).

ST Program - MUL:

The MUL function is used to provide the result of Input 1 divided by Input 2:

Output := Input 1 * Input 2;

Where Output, Input 1 and Input 2 are defined as variables earlier in the ST program. In this case, let's assume Input 1 is 60 and Input 2 is 10. The DIV function returns 600 as 60 x 10=600 (the asterisk * represents the MUL function).

When there are more than 2 inputs, it is more efficient to use the following syntax:

Output := MUL (Input 1, Input 2, Input 3, Input 4 and so on);

For example:

Output := MUL (12, 4, 32, 6);

This would return 9126 as this is the result of 12 x 4 x 32 x 6.


Disclaimer

ClearSCADA 2017 R2