Setting the Default Values

You can assign default values to any of the variables and derived data types. This is useful for programs that need to be set to a specific value prior to them being executed.

You can define default values in a VAR block (in which case, they cannot be overridden) or in a TYPE block (in which case they can be overridden by values in the VAR block).

For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.


Disclaimer

ClearSCADA 2017 R2