Using Logic to Write to a File or Serial Port

You can use the OPEN_PORT and WRITE_FILE functions to write data to a serial port. This is useful for exporting ASCII data to a serial port.

You can also use the WRITE_FILE function to write data to a file.

For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.


Disclaimer

ClearSCADA 2017 R2