Bootstrap Version

Associated with: Lufkin SAMS controllers

This status attribute indicates the version of the controller’s built-in Boot Loader. The attribute is displayed once the controller is or has been in communication with the server.

Also see CPLD Version.


Disclaimer

ClearSCADA 2017 R2