Configure Lufkin SAMS Devices in ClearSCADA

On a ClearSCADA system, you configure the ClearSCADA database so that entries in the database correspond to the plant and measuring instruments on your system. This section summarizes the database items that you need to configure to represent the Lufkin SAM devices on your system.

In order to represent any Lufkin SAM devices, both the Advanced Modbus Driver and the Lufkin SAMS extension component have to be installed and running on the ClearSCADA servers on your system (see Confirm that the Lufkin SAMS Server Component is Installed). When the driver is first installed, a system administrator needs to define the server settings for the driver (see Configuring Lufkin SAMS Server Settings).

When you configure Lufkin SAMS items in the ClearSCADA database, many of the settings for those items need to correspond to the settings of the relevant Lufkin SAM devices on your system. Some settings are either fixed (incorporated into the design of the Lufkin SAM controller), or are configured by an engineer. You need to have access to, or an understanding of, the settings of the Lufkin SAM devices on your system before you can configure the Lufkin SAMS database items successfully. For instance, you need to specify the Modbus address of each Lufkin SAM controller on your system.

You also need to be aware of which optional features are required for each Lufkin SAMS item. These features include:

You can also use core ClearSCADA features with Lufkin SAMS database items, including Lists, Actions, and Mimics. For actions that are specific to the Lufkin SAMS driver, see Actions that are Specific to the Lufkin SAMS Driver. For further information on actions and for details on Lists and Mimics, see the core documentation.

In order for ClearSCADA to retrieve rod pump data from Lufkin SAM controllers, you need to configure:

  1. An Advanced Modbus Channel to represent each communication connection between a Lufkin SAM controller and the ClearSCADA server (see Configuring an Advanced Modbus Channel in the ClearSCADA Guide to the Advanced Modbus Driver).

    With a Direct channel, use the fields within the Scan Groups section of the Scan Parameters tab to specify the frequency with which current data is updated in ClearSCADA (see Define Intervals for Timed Current Data Updates in the ClearSCADA Guide to Advanced Drivers). For Generic Advanced Modbus points associated with Lufkin SAMS devices, the Scan Group interval should be a multiple of the points’ Retrieval Interval rate (see Configure Common Point Properties in the ClearSCADA Guide to the Advanced Modbus Driver).

  2. An Advanced Modbus Outstation Set to define each collection of Lufkin SAM controllers (see Configuring an Advanced Modbus Set in the ClearSCADA Guide to the Advanced Modbus Driver).
  3. A Lufkin SAMS Outstation to represent each Lufkin SAM controller with which ClearSCADA is to communicate (see Configuring Lufkin SAMS Controllers).
  4. A Dynacard Store for each location at the well for which ClearSCADA is to store rod pump readings for a controller (see Dynacard Stores in the ClearSCADA Guide to Advanced Drivers).

    On the Lufkin SAMS driver, each controller supports up to two Dynacard Stores: one to store surface dynacard data, and another to store downhole dynacard data.

  5. A Dynagraph for each type of dynacard data that users are to view as a plot (see Dynagraphs in the ClearSCADA Guide to Advanced Drivers). For example, one Dynagraph to show the Last Stroke measurements, and another Dynagraph to show the latest Shutdown measurements of a particular rod pump.

    You can configure multiple Dynagraphs per type of dynacard. For example, to provide users with different views of the dynacard data.

  6. A Generic Advanced Modbus Point of the appropriate type for each item of current non-dynacard data that ClearSCADA is to retrieve from a Lufkin SAM controller (see Points Used on Generic Modbus Controllers in the ClearSCADA Guide to the Advanced Modbus Driver).
  7. A Lufkin SAMS Point of the appropriate type for each item of historic data that ClearSCADA is to retrieve from a Lufkin SAM controller (see Points Used on Lufkin SAMS Controllers). For example, a Lufkin SAMS Analog Input Point to measure a rod pump’s runtime history.

In addition to the above ‘point’ data, ClearSCADA can also upload the entries from a Lufkin SAM controller’s Event Log on demand (see Upload Event Log).

To minimize the time that it takes to configure the required Lufkin SAMS items, you may want to configure them in the order listed above, as set configuration requires you to specify a channel, and controller (outstation) configuration requires you to specify a set, and so on.


Disclaimer

ClearSCADA 2017 R2