Define the Historic Data Poll Interval

Use the Historic Data Poll Interval field on the Lufkin SAMS tab to specify the frequency with which ClearSCADA retrieves historic point data from the controller.

Enter the interval in the OPC Time Format, or specify 0 to disable automatic polling.


A suitably configured Lufkin SAMS point has to exist in the database for each item of historic point data that ClearSCADA is to retrieve from the controller (see Points Used on Lufkin SAMS Controllers).


Disclaimer

ClearSCADA 2017 R2