Firmware Version

Associated with: Lufkin SAMS controllers

This status attribute indicates the version of the firmware that is running in the controller. The attribute is displayed once the controller is or has been in communication with the server.

Also see Firmware Build Number.


Disclaimer

ClearSCADA 2017 R2